安全基準

安全規格は、AC/DC または DC/DC コンバータの仕様において重要な検討事項です。規格は日々更新されており、その要求事項はアプリケーションによって時には大きく異なることもあります。IT機器の安全性に関するIEC/EN 60950-1は、オーディオ/ビジュアル機器のIEC/EN 60065と共に「デフォルト」規格として多くの製品に適用されてきましたが、2020年12月に完全に廃止される予定です。現在、代替規格であるIEC/EN 62368-1が適用されていますが、最終製品により適した他の規格があるかもしれません。下記にリンクされているZentralverband Elektrotechnik und Elektronikindustrie e.V. (ZVEI)の論文では、適用すべき正しい規格の選択についてのガイダンスが示されています。
Guideline Safety Standards



Selection of safety standards for power supplies

This Guideline on the alternate certification standards after EN60950 is withdrawn was developed by the ZVEI (the German Electrical and Electronic Manufacturer’s Association) with feedback from industry, including input from RECOM. Follow the links below to download the Guide in English or German.