When it comes to an electronically-controlled switch, you want a material that has a high breakdown electric field (e.g. – blocking voltage) when off and very low-resistance conduction channels when on, which is why WBG materials make great semiconducting devices. Some other WBG semiconductors you may have heard of are 
silicon carbide (SiC), gallium arsenide (GaAs), or aluminum nitride (AlN).
  
 
 Fig. 1: Radar Chart Benchmarking Figures of Merit for WBG Materials vs. Si, courtesy of PowerRox [1]
 
GaN also has some other interesting properties that make it attractive for several applications. Its electron mobility and melting point enable high-current channels and higher temperature (or increased reliability at relatively same or lower temperatures), respectively.  
When fabricated into transistors, the resulting devices can have lower gate charge and equivalent on-state channel resistance (RDS_ON) than a Si-based metal–oxide–semiconductor field-effect transistors (MOSFET). Though there are many types of GaN-based switches, let’s focus on the GaN high-electron-mobility transistor (HEMT as an example of one kind,  (its structure is shown in Figure 2).  With the gate activated, current flows very quickly through the shallow GaN layer in what is sometimes called a two-dimensional electron “gas” (2DEG) [2], as represented by the dotted line in the figure.
When Fast is Too Fast
WBG switches can be fast, REAL fast. In fact, they get about as close as you can to the kind of ideal (e.g. – zero transition time) switches we first learn about in textbooks. These speedy transitions are due to the very low gate charge and very high electron mobility properties of materials like GaN. Turn-on and turn-off transitions can occur in <1 nanosecond (1 ns = 10-9 second) even in some fairly high-power applications.  
These transitions are so fast that most engineers trying to measure these transitions on their boards are likely not even using an oscilloscope with the appropriate bandwidth (BW) to sufficiently capture (e.g. – see Nyquist–Shannon Sampling Theorem [4]). If needing to properly measure and characterize a signal with transitions in the nanoseconds, then scope BW needs to be in the GHz range. These kinds of scopes are generally very expensive and usually designed for high-speed data applications rather than power stage analysis.
Gate Drive Challenges
WBG gate thresholds (V
th) tend to be lower than their Si counterparts and with lower abs. max. voltage levels , so the gate drive requirements to take advantage of GaN’s potential also have a fairly steep learning curve associated with designing and implementing such solutions robustly. There are a variety of solutions on the market to address these challenges from integrated gate drives (or even full power stages) to fully-qualified power modules.
This means more care must be taken in the gate drive circuit because we have the risk of shoot-through (or false turn on) due to high transition rates (dV/dt) acting on the switch’s gate-to-source capacitance (a.k.a. – Miller capacitance or C
GS), which can apply a potential to the gate-to-drain capacitance (C
GD) and trigger unwanted turn on. If this occurs when a synchronous device is also on, then a shoot-through (a.k.a. – cross-conduction) event may occur. At best, this will decrease effective efficiency and at worst will lead to the failure of the 
DC/DC converter.
Different kinds of GaN can have differing gate drive requirements and this can be one of the most challenging aspects of designing with GaN components. Some can be driven direct and are normally-off devices, some use what is known as a cascode arrangement in which an enhancement-mode (i.e. – normally-off) MOSFET is used to drive the depletion-mode (i.e. – normally-on) gate of the GaN device. Some can require negative or offset gate drive voltages. For this reason, it can be highly advantageous to acquire a qualified GaN driver, even if designing your own DC/DC solution.
Lots of Resources Out There
There are tons of great resources out there for learning about, acquiring, and implementing GaN solutions. Some of these have already been identified above. Take advantage of them and really do your homework if you are new to WBG and GaN solutions. You will need to go through many build and test iterations to get a truly robust, GaN-based design, particularly for engineers newer to the space.
As a reminder, GaN is not a drop-in replacement for Si and therefore should not be approached as such! The early days of investigating the use of GaN in power supplies involved a lot of people learning this lesson the hard way and even dissuading their opinion of WBG’s viability because of early failures that did not embrace the importance of carefully-managed layout practices and robust gate drive design.
References
[1] E. Shelton, P. Palmer, A. Mantooth, B. Zahnstecher, G. Haynes, “WBG Devices, Circuits and Applications,” APEC 2018 Short Course, San Antonio, TX, March 4, 2018.
[2] Wikipedia contributors, "Two-dimensional electron gas," Wikipedia, The Free Encyclopedia, https://en.wikipedia.org/w/index.php?title=Two-dimensional_electron_gas&oldid=955419012 (accessed May 27, 2022).
[3] “eGaN® Technology," EPC FAQs.  [Online].  Available: https://epc-co.com/epc/FAQ/eGaNTechnology.aspx.
[4] Wikipedia contributors, "Nyquist–Shannon sampling theorem," Wikipedia, The Free Encyclopedia, https://en.wikipedia.org/w/index.php?title=Nyquist%E2%80%93Shannon_sampling_theorem&oldid=1086141927 (accessed May 27, 2022).
[5] “GaN Integration for Higher DC/DC Efficiency and Power Density," EPC Application Note AN018.  [Online].  Available: https://epc-co.com/epc/DesignSupport/ApplicationNotes.aspx.