e-Mobility
The typical applications for e-mobility include electric vehicles (EV), all types of scooters, and similar small vehicles. These devices need battery chargers and on-board power converters for device motor drives and any auxiliary equipment. To replace gasoline-engine vehicles with electric power, a larger network of charging stations and outlets is needed. Currently, approximately 113,600 charging outlets exist in the United States for plug-in electric vehicles along roadways; 36% of them are in the state of California. There is a concerted effort under way to build much faster chargers to lower existing charging times to under 20 minutes.
In more complex products, added features like battery conditioning and bidirectional converters for energy balancing are needed. A solid performance range of suitable AC/DC converters is necessary for these kinds of applications. Battery conditioners (computerized devices that charge, maintain, and prevent sulfation from occurring in lead batteries), along with power-factor front ends, would reduce harmonic distortion (for example from 45% to 5%) and significantly improve system power factor performance. Power factor measures how efficiently the electrical power is being used to perform useful work.
AC/DC e-mobility applications need to be rugged, reliable with long lifetimes, have broad environmental capability with sealed and weatherproof options, power factor correction (PFC), battery charging/conditioning capability, and 20kW+ rating. High power AC/DC converters can be used for special applications. One typical example is an AC/DC converter that can operate at nominal 44V or 24V three-phase AC input while providing a 28V or 14V capability at either 2.8kW or 1.4kW. Other AC/DC devices are battery chargers/conditioners specially designed for the e-mobility market, which is categorized by battery voltages of less than 24V, 24V, 36V, 48V, and even greater than 48V. The 24V segment typically accounts for more than 25% of the electric mobility revenue share. These AC/DC converters are rated at 2kW and 1kW, respectively, with excellent wide output operating voltage ranges to enable designers with flexible applications.
In this segment, some AC/DC converters have modular standalone power factor correction front ends that are also available rated at 800W, 1600W, and 3200W (single-phase AC input) and at 4kW (three-phase AC input). Some of these AC/DC solutions fit into designs in a 19-inch rack, open-frame or chassis formats. Other key applications for these AC/DC converters in e-mobility are EVs and EV charging systems, with the addition of railway and transportation.