For devices with fixed internal power dissipation and ambient temperature limits, as is common in most power conversion devices and ICs, the surface temperature of the case depends on the internal thermal resistance and the efficiency of heat transfer to ambient. Internal thermal resistance measures how effectively heat is conducted from the source to the device surface.
When discussing thermal management, the focus is often on a component’s effectiveness in transferring heat to ambient – via convection, conduction, and/or radiation. These methods often rely on passive heat exchangers, fans, liquid cooling systems, heat pipes, heat sinks, and similar solutions.
Therefore, the best way to maintain an acceptable case temperature is to optimize both the internal thermal resistance of the device and its heat transfer to the ambient environment. A thermally ideal device would have zero thermal resistance and infinite heat dissipation to the environment. However, since components are made from real-world materials – each with unique thermal resistance properties – and no system can perfectly transfer heat, designers must optimize the thermal performance of every critical component from the earliest stages of design.