A sensor typically needs just a few watts to operate at a low voltage, down-converted from the main system rail using a DC/DC converter. The system rail nominal is often 110VDC but sometimes is as low as 24V. Power requirements can be higher though in multi-channel sensor arrangements or when actuators have to be driven, perhaps up to about 40W.
Individual isolated DC/DCs are normally employed for each sensor to keep output voltage drops low and to avoid ground loops which might cause EMC problems such as sensor cross-interference. The system supply rail however is not ‘clean’. Standard EN 50155-2017 allows a variation of +25%/-30% in normal operation with dips to 60% and surges to 140% of nominal for 100ms with no ‘deviation of function’ allowed and 125% to 140% of nominal for one second with performance degradation. To cover these variations, DC/DC converters for 110V systems must typically operate from 43 to 160VDC.
Fast transient overvoltages are also present on the system rail as defined in the EN 61000-4-x series of standards, however suppressors and simple LC filters can attenuate these. Complete loss of supply can also occur though; EN 50155 defines interruptions in two classes S1 and S2 with the worst being 10ms loss of supply from nominal input with no degradation in performance. For some equipment the interruption can be 30ms on supply change-over (Class C2). To cover this, hold-up capacitance external to the converter is normally added after a series isolating diode, which can also provide reverse polarity protection – another requirement from the standard.
An example application is shown in Figure 1 where a fan is activated by a carriage temperature sensor, with temperature and status signalled via a WLAN connection. A RECOM 8W DC/DC converter is shown with an input range of 43 to 160V providing a regulated, isolated, 5V power rail for the sensor circuitry. The DC/DC is very compact at just 32 x 20 x 10mm. Extended hold up and reverse polarity protection is shown along with an optional EMI filter for high immunity to transients and low conducted emissions although the RECOM DC/DC already has high compliance levels to rolling stock EMC standard EN50121-3-2.