WPT is a popular choice in numerous applications. Its popularity spans consumer electronics, ranging from smartphones to electric toothbrushes. Moreover, in the
medical field, WPT plays a critical role in powering implantable devices like pacemakers and insulin pumps. Industrial sectors also benefit from WPT technology, with its integration into power tools,
automatic guided vehicles (AGVs), and beyond.
Foreign Object Detection (FOD). A metal object, such as a coin, a key, or a nail, may be inadvertently located near the magnetic fields generated by the WPT system, creating a potential safety hazard and affecting the electrical characteristics of the WPT system. High magnetic fields may also produce adverse symptoms in living objects located between the transmitter and receiver. Identifying such unintended objects and avoiding transmitting power to them is known as foreign object detection (FOD). FOD is typically accomplished by calculating the power received at the receiver and communicating it back to the transmitter. A mismatch in the two values after correction factors have been applied is assumed to be due to a foreign object absorbing power and triggers a shutdown.
Communication and Control. WPT systems typically use communication interfaces to exchange information between the transmitter and receiver such as load requirements or system status. This facilitates intelligent power management and control. Qi receivers use amplitude shift keying (ASK) to communicate power level requests and for FOD detection; Qi transmitters use frequency shift keying (FSK). Resonant WPT systems meeting the AirFuel standard use a protocol derived from the popular Bluetooth Low Energy (BLE) standard.
In addition to wireless communication between the transmitter and receiver, the power supply should also include a wired digital interface such as PMBus. This feature allows the control system to optimize the power supply voltage for peak performance, and the power supply can transmit status information, error codes, and other parameters.
Electromagnetic Compatibility (EMC). The power supply should comply with electromagnetic compatibility standards to prevent interference with other electronic devices and ensure the reliability of the overall WPT system.
RECOM products suitable for wireless power transfer applications
As mentioned above, an ideal power supply for WPT use should be well regulated, both for line and load variations, efficient, isolated, protected (SCP, OVP, and OTP), and meet the relevant EMC requirements.
RECOM offers many
AC/DC power supplies that meet these requirements. The
RACM600-L series, for example, can provide 450W continuous power (up to 800W peak) and offers a PMBus interface. The
RACM1200-V supplies up to 1000W fan-less power with 1200W boost power available for up to 10 seconds, again with a
PMBus option. Custom variants are also available.
Power supplies in wireless power transfer applications need to meet a combination of stability, efficiency, safety, and compatibility requirements to ensure seamless and reliable power transfer in diverse scenarios ranging from consumer electronics to industrial applications. The design considerations for WPT power supplies are crucial in advancing the adoption of wireless charging technologies.
RECOM has some valuable training material for those wanting to learn more about this fast-changing field. Our
AC/DC Book of Knowledge contains much information about some of the basic physics and practical design techniques applicable to WPT. And RECOM design engineers are always available to discuss
custom design projects.