Gmunden

Headquarter, R&D, Tech Support, Supply Chain Management, Marketing, Accounting, Distribution

Power Electronics for the world market from the heart of Europe

The RECOM group in Gmunden, Austria, has built a campus-like headquarters site with a total of three thousand square metres of floor space in a bid to intensify the company’s commitment to the electrical power supply. In addition to a modern logistics centre and new management facilities, RECOM has placed special focus on its labs, extending the R&D, testing, investigation and quality assurance labs by a state-of-the-art EMC lab; this comes as a substantial boost to the company’s capabilities in the high-frequency range serving Austria and southern Germany.

The 3m-SAC (semi-anechoic chamber) equipped by Rohde & Schwarz will see standard-compliant measurements performed at a frequency range of 30 MHz to 3 GHz according to CISPR22. The SAC features an automated measurement procedure on test pieces at up to one metre in diameter, and the computer-controlled turntable and near-field probes allow fully automatic determination of critical interference sources in each test piece.
Apart from that, the laboratory is equipped for measurements according to EN 61000-4-x and EN 61000-3-2, the latter playing an especially important role in LED drivers. The in-house GTEM cell can also examine the test piece’s behaviour for radiated immunity. RECOM has set aside separate rooms at the RECOM campus as well as three studio flats for visiting students and researchers to facilitate closer cooperation with universities, colleges and other higher-level academic institutions.

RECOM customers and partners can also use the company’s highly equipped labs to test their own prototypes. Close cooperation with other companies in the electrical power supply sector is set to develop into an innovative electrical power supply cluster between Munich, Linz and Graz in the long term.

Address

Münzfeld 35
4810 Gmunden
Austria
+43 7612 88 325 700
+43 7612 88 325 801
info@recom-power.com

Directions